SUG_Wiser_Denmark_WSE-09

Ethernet mode connection- Gateway

  1. Locate the Ethernet port (A) on the gateway.
  2. Connect an Ethernet cable between the gateway and the router to suit the installation method used for the gateway:
You must add the gateway to the app before you can add devices to control them. To do this, first download and install the app on your mobile phone/tablet (see Downloading the app ) and register a user account. You can then add the gateway and optionally connect the gateway to the network router by Wi-Fi.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.