SUG_Wiser_Denmark_WSE-09

Device button/key and LED locations

Find the location of buttons, keys and LED indicators on various devices.

Wiser Wireless Relay/Wireless Shutter Control for build in (puck)

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

Wiser Wireless Dimmer for Build in (puck)

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

(See A) Setup/Reset button. Press 3 times on the rocker to activate.

(See B) Status LED

LK FUGA® Wiser Wireless Double Relay/Wireless Dimmer

(See A) Setup/Reset button

(See B) Status LED

LK FUGA® Wiser Wireless Battery 4 Button Switch

(See A) Button (1)

(See B) Status LED

Wiser Wireless Door and Windows Contact Kit

(See A) Function key

(See B) Status LED (visible on front of master part when flashing or lit)

Wiser Wireless Ceiling PIR

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser Wireless Leakage Sensor

(See A) Function key

(See B) Status LED (visible on top of sensor when flashing or lit)

Wiser Wireless Temperature and Humidity Sensor

(See A) Function key

(See B) Status LED (visible on sensor face when flashing or lit)

Wiser SmartPlug 16 A

(See A) Operation button

(See B) Status LED

Wiser IP Camera Indoor

(See A) Micro SD Card slot

(See B) Status LED

(See C) Reset Button

Smoke Alarm Battery/ Wiser Smoke Alarm 230 V /

(See A) Reset button

(See B) Standby LED

(See C) Status LED

Wiser Radiator Thermostat

(See A) Function Knob

(See B) 3 status LED

PowerTag Energy

(See A) Status LED

Connected Motion Sensor with Multiwire Dimmer

(See A) Status LED

(See B) Reset Button

Wiser Adapter

(See A) Push button and Status LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.