SUG_Wiser_Denmark_WSE-09

Adding a Wireless battery switch to a Room Control network

Before using the Wireless battery switch as a remote controller, it must first be added to a Room Control network.

To perform adding Wireless battery switch, the target Room Control Network should be OPEN state first. In a Room Control network the Wireless battery switch works as a Sender but not as a Receiver.

NOTE: When the wireless switch is paired to the Wiser Gateway, it is automatically set to 2-channel mode. Further setup of the device is done in the Wiser App.
  1. Remove the rockers and cover plate from the Wireless battery switch.
  2. (See B, C) Short press the button (1) at top-left of device (B) 3 times.
    The status LED (C) blinks amber and then turns green upon successful connection to the Room Control network.
    TIP: To save the battery, the green LED in the Wireless battery switch turns off after a few seconds, but the Wireless battery switch remains in Room Control network.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.