SUG_Wiser_Denmark_WSE-09

Supported Wiser devices

The devices listed in the following table are available for use in the Wiser system.

Follow the device Installation Instructions links for device installation instructions.

IMPORTANT: These devices must not be used in safety applications and are only for general residential use only.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.