SUG_Wiser_Denmark_WSE-09

Removing a Room Control group

Remove the link between Sender devices and related Receiver devices when the Room Control group is no longer needed.
IMPORTANT: Only perform this task where there is no gateway network.
  1. On the Sender device, short-press the device button 3 times then press and hold the button for 6 seconds. (Refer to the device user manual-see links to the user manuals in Supported Wiser devices.)
  2. Release the device button when the device LED blinks green at 6 s.
    NOTE: All bindings between the Sender and Receivers are removed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.