SUG_Wiser_Denmark_WSE-09

Dimmers

LK FUGA®Wiser Wireless Dimmer

Controls the lighting level in a room, or automatically set lighting to a desired level in response to a specified condition or event.

LK product catalog

Instruction Sheet (PDF)

Wiser Wireless Dimmer for Build in (Puck)

Converts compatible mechanical push-button switches into smart dimmers. Connect up to 10 compatible mechanical push buttons.

NOTE: Mechanical push buttons must be certified for use in 220–240 V AC applications.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

LK FUGA® Wiser Wireless PIR with Dimmer

LK FUGA® Wiser wireless PIR dimmer with neutral

Detects moving heat sources (e.g. persons) and can dim ohmic, inductive or capacitive loads and switch them on for a adjustable overtravel time.

LK product catalog

Instruction Sheet (PDF)

Instruction Sheet (PDF) (With Neutral)

Device User Guide

LK Fuga® Wiser Multiwire LED Rotary Dimmer

Controls the lighting level in a room, or automatically set lighting to a desired level in response to a specified condition or event. Can switch and dim ohmic, inductive or capacitive loads.

LK product catalog (without center-plate and knob)

LK product catalog (with center-plate and knob)

Instruction Sheet (PDF)

Device User Guide

Wiser Multiwire Micro Module LED Dimmer

The Wiser Multiwire Micro Module LED Dimmer combines the advantages of smart dimmer functionality with ordinary mechanical push-button switches.

NOTE: Mechanical push buttons must be certified for use in 220 – 240 V AC applications.

LK product catalog

Instruction Sheet (PDF)

Device User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.