SUG_Wiser_Denmark_WSE-09

Room Control

In a Room Control network, one or more groups of devices can be configured for remote control operation.

Within each group, devices can be configured as Senders (see A) and/or Receivers (see B).

A simple Room Control group using compatible devices

NOTE: Puck devices, relays, and dimmer LK FUGA® Wiser wireless double relay and LK FUGA® Wiser wireless dimmer can only be configured as receivers and battery switch can only be configured as sender.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.