SUG_Wiser_Denmark_WSE-09

Creating a network for Room Control

Create a network of compatible devices where there is no gateway network.
IMPORTANT: Do not perform this task if a gateway network is present. Compatible devices that are already part of a gateway network can be configured for Room Control. See Creating a Room Control group.

Important information for puck devices:

WARNING
Danger due to electric shock
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Create a new open network. Select a mains-powered device and short-press the button 8 times. The device LED displays solid green once the network is created.
    TIP: It can take a minute or longer to create the network. During this time there is no indication that anything is happening which can give the appearance that the action has not been achieved. However, this is not the case.
  2. Add more devices to the network. Short-press each device button 3 times. The device LEDs blink amber while joining the network, then steady green once joined successfully.
    TIP: In the diagram, #1 signifies first device (i.e. the one used to create the Zigbee network). #2 ~ are the other devices added in the group.
  3. Close the network. On any device (except the wireless battery 4 button switch), short-press the device button 8 times.
    TIP: The network closes automatically after 180 seconds if you do nothing.

Creating a Room Control network and adding devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.