DUG_Renova - ZB Thermostat 16 A_WSE-00

Child lock settings

The child lock helps to prevent children from operating the thermostat. When the Child Lock is enabled, thermostat can be operated only using the app.

To enable/disable the child lock:
  1. On the Home page, tap All devices > Thermostat.
  2. Tap Settings.
  3. Tap the toggle switch (A) to enable/disable the Child Lock settings.

    NOTE: By enabling the child lock, thermostat can only be controlled using the app and not change the temperature setpoint value using physical device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?