Managing device settings using Wiser app
To access the settings:
-
On the Home page, tap All devices > Thermostat.
-
On the device control panel page, tap Settings.
All setting option in the Wiser app is based on the preset value set during paring process.
Preset |
Valve protection |
Air calibration setting |
Sensor type selection |
Floor calibration setting |
Max/Min guard temp. setting |
Child lock |
Rated power value |
Screen brightness settings |
P1 | ü | ü | x | x | x | ü | x | ü |
P2 | ü | ü | x | x | x | ü | x | ü |
P3 | ü | ü | ü | ü | ü | ü | x | ü |
P4 | x | ü | x | x | x | ü | ü | ü |
P5 | x | ü | ü | ü | ü | ü | ü | ü |
P6 | x | ü | ü | ü | ü | ü | ü | ü |
P7 | ü | x | ü | ü | ü | ü | x | ü |
P8 | x | x | ü | ü | ü | ü | ü | ü |
P9 | x | x | x | x | x | ü | ü | ü |
Below are the setting interface based on preset: