DUG_Renova - ZB Thermostat 16 A_WSE-00

Setting the room temperature using app

By using the Wiser app, you can control the room temperature.

To control the room temperature:

NOTE: You can only adjust the room temperature through the control panel of the group thermostat.

  1. On the Home page, tap All devices > Thermostat.

  2. On the control panel page, you can do either of the following to adjust the temperature (A):

    – Tap “+” or “” sign to set the temperature setpoint.

    – Drag the sliding bar up/down to set the temperature setpoint.

    NOTE:
    • The thermostat setpoint temperature ranges from 4 °C~ 30 °C for preset P1 – P6 and 10 °C ~ 40 °C for preset P7 – P8.

    • Each “+/–” tapping will increase or decrease the setpoint temperature by 0.5 °C.

    TIP: Tapping you can set the boost time and turns it off.

Heating mode: When the thermostat is in heating mode, flame icon is displayed in the Wiser app.

NOTE:
  • The indicates that the room temperature is below the desired temperature (set point), so the heating is on.
  • The indicates that the room temperature is above the desired temperature (set point), so the heating is off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?