DUG_Renova - ZB Thermostat 16 A_WSE-00

Setting boost mode manually

You can enable and disable boost mode manually.
When enabled the temperature increases by 2° C for temperature control modes (P1 to P8) and by +2 for regulator mode (P9) over the setpoint.

To enable boost mode:

  1. Press O button once to enter boost menu.


    +1 flashes on thermostat matrix.
  2. Use +/- button to navigate between the boost hours from +1 to +3.

    After selecting the boost hours, thermostat will save and exit boost mode if there is no interaction within 5 s.

For example:
If current setpoint is 12° C and you enable boost mode by selecting +3.
The boost mode will set the setpoint temperature to 14° C for next 3 hours. After 3 hours setpoint will return to 12° C.


To disable boost mode:

  1. Press O button once.
    +1 flashes on thermostat matrix.

  2. Press + button for thermostat to display – – (boost cancel).

    After selecting the boost cancel, thermostat will save and exit boost mode if there is no interaction within 5 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?