DUG_Renova - ZB Thermostat 16 A_WSE-00

Screen brightness settings

You can increase/decrease the LED brightness on the thermostat using the app.

Active brightness level

You can configure the brightness of the LEDs when the thermostat is active (during interaction):

  1. Tap Active Brightness Level (A).

  2. On the slide up menu, adjust the desired brightness level then tap Save.

NOTE:
  • Default active screen brightness is 100%

  • The screen brightness range is 1%~100%, and the setting accuracy is 1%.

Idle brightness level

You can configure the brightness of the LEDs when thermostat is inactive (after time-out of screen active brightness).

  1. Tap Idle Brightness Level (B).

  2. On the slide up menu, adjust the desired brightness level then tap Save.

NOTE:
  • Default idle screen brightness is 0%

  • The screen brightness range is 0%~100% and it should not be more than active brightness level.

Screen active duration

The thermostat can be configured to set a timeout for the LED when it is active.

  1. Tap Screen Active Duration (C).

  2. On the slide up menu, select required active duration:

    • 5 Secs

    • 10 Secs

    • 30 Secs

    • 45 Secs

    • Customized Duration: use +/- or drag the sliding bar to change the Active Duration, which ranges from 1 minute to 60 minutes.

      NOTE: Default screen active duration is 60 s.
NOTE: In the event that the thermostat is removed from the system, the brightness setting will be retain.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?