DUG_Renova - ZB Thermostat 16 A_WSE-00

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when it is powered on.
  1. On the Home page, tap +.
  2. Tap Auto scan > Confirm.
  3. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser HUB from the slide-up menu.
  5. Long press the O button until 'Jn' is displayed and then release the button to initiate joining.
    NOTE: If you have already paired your thermostat, and want to change the preset mode during the current pairing process, you will need to perform a factory reset. Otherwise, the thermostat will be paired with the previous preset mode. Refer resetting the device.
    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds.
  6. Wait for a few seconds until the device search is complete, than tap Next (A) and select Thermostat 16 A.
  7. Once the device is paired successfully, assign a room to enable settings and than tap Done.
    NOTE:
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?