DUG_Renova - ZB Thermostat 16 A_WSE-00

Resetting the device

You can manually reset the thermostat to factory settings or soft reset.

Soft reset

Press and hold the O touch button > 20 s.

The thermostat flashes “Sr”, indicating soft reset, and it is selected when the button is released.
The ‘Sr’ will flash to confirm the soft rest.
NOTE: To cancel the soft reset, press and hold the O button for > 30 s. This reverts the thermostat's UI back to its previous state before the touch button is pressed, with no change in a functional state.

A soft reset will:

  • Delete all cloud and account details maintained by the device to allow re-registration.

  • Revert to the default setpoint in manual control.

  • Maintain all Factory settings e.g. MAC address.

  • Maintain the installer configuration of the device to ensure proper functioning until and after rejoining/re-registration.

Factory reset


In reset selection, press and hold the O touch button until thermostat flashes “Fr”, indicating factory reset, and it is selected when the button is released.
The ‘Fr’ will flash on the matrix display to confirm the factory reset and the thermostat resets to factory defaults and after 5 s it returns to preset.

NOTE: To cancel the factory reset, press and hold the O button for > 30 s. This reverts the thermostat's UI back to its previous state before the touch button is pressed, with no change in a functional state.

A factory reset will:

  • Delete all configuration data.

  • Delete all schedules information.

  • Revert to the default setpoint in manual control.

  • Maintain all Factory settings e.g. MAC address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?