DUG_Renova - ZB Thermostat 16 A_WSE-00

Valve protection settings

Hydronic underfloor heating and boiler connections require valves and protection, while electric underfloor heating does not use valves. This feature can only be used in hydronic applications.

Valve protection

The valve protection can be enabled or disabled by tapping the toggle switch (A) on the valve protection setting.

NOTE: Activate output every two weeks to prevent valve calcification. It only supports Enable/Disable feature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?