DUG_Renova - ZB Thermostat 16 A_WSE-00

Pairing device manually

The device can be paired manually by scanning the installed code or entering it manually during pairing.
  1. On the Home page, tap +.
  2. Tap and select the required Wiser HUB on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code
    TIP: It is highly recommended to add the device with Install code.
  4. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code.
    • Enter Install Code Manually - you can manually enter the install code from the device.
    After pairing the device with install code, proceed to Step 6.
  5. To pair the device without install code, tap Add Device without Install Code.
  6. Long press the O button until Jn is displayed and then release the button to initiate joining.
    NOTE: If you have already paired your thermostat, and want to change the preset mode during the current pairing process, you will need to perform a factory reset. Otherwise, the thermostat will be paired with the previous preset mode. Refer resetting the device.

    "Jn" will flash on the matrix.
  7. In the app, tap Confirm device display Jn and than tap Start Configuration (C).
  8. Wait for a few seconds until the wireless LED on the thermostat turns green.
  9. After the device is added in the app, assign a room to enable settings and than tap Done.
    NOTE:
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?