Device presetting
*PI (Proportional and Integral) controller is a commonly used method in control systems to correct for error between the commanded setpoint and the actual value based on some type of feedback
You can choose one preset configuration:
| Preset | Configuration | Control type / Set point range | Cycle time* (min) |
| P1 | Heat Pump/Oil Boiler | Room
Control 4°C ~ 30°C |
20 |
| P2 | Hydronic Radiator/Gas Boiler | 10 | |
| P3 | Hydronic Underfloor | 10 | |
| P4 | Electrical Radiator | 10 | |
| P5 | Electrical Underfloor (Without floor limits) | 10 | |
| P6 | Electrical Underfloor (With floor limits) | 10 | |
| P7 | Hydronic Underfloor | Floor
Control 10°C ~ 40°C |
10 |
| P8 | Electrical Underfloor | 10 | |
| P9 | Regulator Mode (output displayed is based on percentage) | Floor
Control 0 ~ 10 (0% ~ 100%) |
30 |
**Cycle time: This setting determines the length of each on/off cycle of the output relay. In a cycle time, the time interval between relay cycle is based on the demand setpoint. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor. A short cycle time is more appropriate for faster heating surfaces, such as an electric panel heater.
Initial preset configuration (by default)
When the thermostat is first powered on or immediately after a factory
reset, by default “P5” flashes on the matrix
LED’s if there is no external sensor connected, or “P8” if there is any external sensor connected.
Modifying the preset value
To modify the preset from default value, simultaneously
press "O" and "+" for 10 s to enter advanced settings
menu. Then press + button on the thermostat, it increases the
preset value by 1 and when – button is pressed, it decreases
the preset value by 1.
For example, when + button is pressed, preset P1 becomes P2, continue
to press the + button, and the preset changes to P3, P4...P9.
Similarly, when – button is pressed, preset P9 changes to P8, continue to press the – button, preset changes to P7, P6...P1.
Confirming the preset
Select the preset that meets your needs using the +/- buttons,
and then hold the O for > 1 s to confirm the selection.
For example, P1 is confirmed.
-
Cycle Time : 20 mins
-
Valve Protection : Off