DUG_Renova - ZB Thermostat 16 A_WSE-00

Removing the device from Wiser system

You can remove a device from the device list using the Wiser app.
  1. On the Home page, tap All devices and select the individual Thermostat which needs to be removed.
  2. Tap to display more details.
  3. Tap Remove Device (A) and tap Confirm.
    NOTE: Setting parameters will be retained when the thermostat is removed from the Wiser system.
    TIP:
    • On the home page, you can tap and hold the individual thermostat to remove the device.

    • In group thermostat, tap for more information and then tap Remove Device to remove the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?