DUG_Renova - ZB Thermostat 16 A_WSE-00

Example of an automation

This demonstration shows you how to create an automation to turn on the thermostat setpoint to 20 °C when the outdoor temperature is less than 15 °C .
  1. Go to Automation > + to create an automation.
  2. Tap Edit name , enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When weather changes > Outdoor Temperature.
  4. Select the outdoor temperature value (A), the condition (B) and tap Next.
    TIP: You can set the outdoor temperature value as 15 °C and the condition as < (less than).
  5. Tap Add task > Run the device and select Thermostats.
  6. Tap Thermostat Set Point and set the temperature as 20 °C (C).

  7. In the Automation Settings page, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?