DUG_Renova - ZB Thermostat 16 A_WSE-00

Sensors settings

Temperature detection

You can check the sensor type (A) under temperature detection, based on your preset.

Air Temperature: for preset P1 to P6.

Floor Temperature: for preset P7 to P8.

NOTE: Sensor settings are not available for regulator mode (P9).

Temperature calibration

To set the temperature calibration:

  1. Tap Temperature Calibration (B) for a slide-up menu.

  2. Drag the sliding bar or use –/+ button to set the temperature calibration.

    NOTE: The temperature calibration ranges from -9°C to +9°C and can be adjusted in 0.1°C increments.
  3. Tap Save.

Floor sensor type

To select the floor sensor type:

  1. Tap Floor Sensor Type (C) for slide up menu.

  2. Select the sensor type (kOhm) form the following list.

    • 10K

    • 12K

    • 15K

    • 33K

    • 47K

    NOTE: Select correct floor sensor type which is installed and then you can set calibration and guard temperature.

Guard temperature

To set the maximum and minimum guard temperature:

  • On setting page, tap Max Guard Temperature (D) to set upper temperature limit of the floor sensor and then tap Save.

    NOTE: The temperature ranges form 21°C to 40°C and maximum guard temperature should be higher than minimum guard temperature

  • Tap Min Guard Temperature (E) to set lower temperature limit of the floor sensor and then tap Save.

    NOTE: The temperature ranges form 5°C to 19°C and minimum guard temperature should be lower than maximum guard temperature

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?