LED Indications
Pairing the device
Presetting the device
|
Status |
User Interaction |
Description |
|
Enter preset selection |
By default, thermostat matrix display flashes “P5” if there is no external sensor connected, or “P8” if there is any external sensor connected when the thermostat is first powered on or after a factory reset. |
|
|
Modify preset selection |
The default preset value can be modified by simultaneously pressing "O" and "+" for 2 s to enter advanced settings menu In advance setting menu the thermostat matrix display flashes "P1" or "P2...P9" when +/– button is pressed. Note: When + button is pressed, preset increases by one; similarly, the preset decreases by one when the – button is pressed. For more information, refer to the section presetting the device. |
Setting a sensor type
Resetting the device
|
Status |
User Interaction |
Description |
|
Soft reset |
A solid "Sr" LED is displayed on the thermostat matrix display until the user releases the O button, then "Sr" flashes. For more information, refer to the section Resetting the device. |
|
|
Factory reset |
A solid "Fr" LED is displayed on the thermostat matrix display until the user releases the O button, then "Fr" flashes. For more information, refer to the section Resetting the device. |
Showing demand - temperature control modes
|
Status |
User Interaction |
Description |
|
Heating demand |
Temperature display
|
Status |
User Interaction |
Description |
|
Temperature below minimum display
value |
Note: The thermostat matrix displays temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “--” When the temperature is below -9 degrees. OR The thermostat matrix display flashes “--” when the thermostat cannot determine the temperature due to an error. |
|
|
Temperature above maximum display value |
Note: The thermostat matrix displays temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees. |