DUG_Renova - ZB Thermostat 16 A_WSE-00

Turning on/off the device manually

When thermostat is not in use, you can turn on/off the device manually
NOTE: Make sure to disable childlock before turning off the device.

Press for > 10 s to turn off.

When thermostat is fully off:

  • LED displays no room temperature

  • Does not control room temperature

  • Outputs remain off

  • On initial interaction, the device shows an “X” on the display to show that it is off.

Wake the thermostat by pressing /O/+ once, thermostat matrix display X and then press /O/+ button for > 5 s to turn.

When the thermostat is turned on, it returns to its last state.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?