DUG_Renova - ZB Thermostat 16 A_WSE-00

Rated power settings

The thermostat does not include any hardware to monitor the power output of the heating load. To provide power monitoring functionality, the rated power value (W) of the connected heating load needs to be entered in the app. You can view the power consumption (W) on the app.

Rated power value

To monitor instant power value information in the app:


– Tap Rated Power Value

– On the pop-up menu enter the rated power value (A) and then tap Save (B).


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?