SUG_SV_FI_WH-04

Dynamic Tariff

To set Dynamic tariff:
  1. After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.
    NOTE: If you have already configured your tariff settings, follow below menu navigation if you need to modify tariff rate.
    On the Home screen, tap > Energy Management > Tariff > Electricity.
  2. Tap (A) and select Dynamic.
  3. Tap (B) to set the contract limit.
    IMPORTANT: Contract limit is already set when pairing the main PowerTag as Grid. Refer to Pairing the main device .
    1. Select your contract limit (kVA/A/kW) size from the dropdown menu, then tap and enter a value using the dial pad as per your country.
      TIP: Default value is 20 A with range of 16–63 A.

      A notification window will be prompted that the Contract Limit is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping. Tap Continue, if you like to proceed.

      IMPORTANT: Anti-Tripping is applicable only if you have installed Water Heater/EV Socket/Schneider Charge/EVlink Home Smart in your home.
      For more details, refer to Anti-Tripping (Add Link).
    2. Tap after setting the contract limit.
  4. Tap (C) and select a subscription type (D) (refers to recurrent fee).
  5. Enter a value in the Cost (kr)(E) field and tap Set.
    TIP: The Fixed Charges is applied to recover the basic cost of electric service, independent of how much energy is used. These charges are electricity costs that don't change no matter how much electricity you use. This amount is fixed in your electricity bills.
  6. Tap (F) and select the tariff zone based on your location.
    NOTE:
    • A tariff zone is a designated area where the same energy pricing rules apply. It is used to reflect regional costs and manage electricity distribution. This information appears on your electricity bill.

    • We only consider the spot-price and not the full tariff. Therefore, the actual electricity bill may differ.

    • If you don’t know your tariff zone, tap Find your tariff zone (G) to find your tariff zone using the map.

  7. Tap Save once the details are entered.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.