SUG_SV_FI_WH-04

Home Screen Settings

The Wiser Home App offers options to customize the Home Screen.

Find the Home Screen options in the Settings Menu.

Setting

ON

OFF

Start on Control Tab

The App opens directly in the Control tab.

The App will open on the Home Screen.

Show Moments

The List of available Moments is shown in the upper part of the Home screen.

Moments will not be shown on the Home Screen.

Show Tips and Advice

Helpful tips and advice are displayed on the Home screen.

Tips and advice are hidden from the Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.