SUG_SV_FI_WH-04

Safety & Security

Wiser Smoke Alarm - Battery

CCT599001

The Wiser Smoke Alarm - Battery uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat caused by rapid increase in temperature. When connected to the Wiser system, the device sends notifications to the user via the Wiser app.

Instruction Sheet (PDF)

Device User Guide

Wiser Smoke Alarm 230 V

CCT599501

The Wiser Smoke Alarm 240 V Square uses a photoelectric sensor to detect smoke generated by fire and a temperature sensor that detects heat caused by rapid increase in temperature. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the Wiser system, the device will send notifications via the Wiser app.

Instruction Sheet (PDF)

Device User Guide

Wiser Window/Door Sensor

CCT591011

Can be used to detect if a door or window is opened or closed.

Instruction Sheet (PDF)

Device User Guide

Wiser Motion Sensor

CCT595011

Reports the detection of movement and measures the luminance of the environment.

Wiser Water Leakage Sensor

CCT592011

Detects water on a surface.

Instruction Sheet (PDF)

Device User Guide

Wiser Temperature/Humidity Sensor

CCT593011

Measures temperature and humidity

Instruction Sheet (PDF)

Device User Guide

ARGUS Motion Sensor Outdoor 360

CCT564114

CCT564119

It offers advanced motion detection, LUX measurement, and temperature sensing capabilities. It allows you to automate and enhance your smart home environment effortlessly.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?