SUG_SV_FI_WH-04

Using Wiser Home AI

Using the Wiser Home app, you can view how the devices are controlled and scheduled for usage.

Device Control screen

On the device control screen:

A

Indicates the next scheduled time for the device to switch On.

B

Displays the load activation schedule for the next 24 hours.

NOTE: Scroll through the options to view the complete schedule.

Schedule

You can change the schedule mode to Wiser Home AI any time.

  1. Tap (C) to open the sub-menu.

  2. Tap (D) to switch the schedule mode to Wiser Home AI.

Away Mode

If you wish to activate Away Mode with Wiser Home AI. Away Mode will override Wiser Home AI commands for smooth home adaptation when you are away. For more information on Away Mode, refer to .Away Mode

Insights

In > Insights you can find details about the upcoming schedule for your Wiser home AI enabled devices.

NOTE: (E) Provides real-time alerts and recommendations to notify you of any irregularities, feature malfunctions, or optimization opportunities. These notifications help you take timely action, ensure maximize overall performance and energy efficiency.

To view how much money is saved through Wiser Home AI, refer to Insights.

NOTE: Savings will be shown as per what offer you have opted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.