Appliances
|
Connected Wireless Switch 1-gang/ 2-gang WDE002906 WDE002924 |
The Connected Wireless Switch 1-gang/2-gang is used to control a group of Zigbee devices within the same Zigbee network. The device can be configured through the Wiser app or can be paired with other Wiser Zigbee devices. |
|
|
Wiser Power Micromodule CCTFR6730 |
The Wiser Power Micromodule is for switching loads (up to 3000 W resistive) such as a hot water tank or a socket outlet. In combination with the Wiser app, the energy consumption can be measured and the module can be used for load shedding or demand response. |
|
|
Connected Single Socket Outlet 16A WDE002172 |
Remotely controls and monitors the power consumption of the plugged-in load. |
|
|
Wiser SmartPlug 16 A CCT711119 |
Controls various electrical devices, for example floor lamps, radios, ventilators or coffee machines, using the app. Monitor energy consumption of plugged-in devices. |
|
|
Double Socket Outlet 16A WDE002182 |
Consists of a smart and standard outlet. The upper smart socket controls and monitors the plugged-in power. The lower standard socket provides uncontrolled and unmonitored power. |