SUG_SV_FI_WH-04

Setting-up Overconsumption Alarm

This topic explains how to setup an overconsumption alarm for a device.
  1. On the Notifications and Alarms screen, tap Create a new alarm (A).
  2. Choose alarm type as Overconsumption (B).
  3. Select the device from the device list and tap Next (C).
  4. Tap icon (D) and set the power consumption limit that you consider normal for the selected device during its normal operation.
  5. Tap icon (E) and set the duration for which the device should be operating above the set power consumption limit before triggering an alarm.
  6. Once you have entered the desired values for both the maximum power consumption and the duration, tap the Save (F).
  7. To delete an alarm, select the device and tap Delete (G).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.