SUG_SV_FI_WH-04

Climate

Wiser Radiator Thermostat

CCTFR6100Z3

Provides individual temperature control for radiators.

Instruction Sheet (PDF)

Device User Guide

Wiser Room Thermostat with display

CCTFR6400

CCTFR6401

Wireless, battery-powered, colored touch-button display to set the room temperature.

Instruction Sheet (PDF)

Device User Guide

Exxact - Connected Thermostat Room/Floor 16 A

WDE002497

WDE003497

The Connected Thermostat Room/Floor 16 A is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water-based heating.

Instruction Sheet (PDF)

Device User Guide

Renova - Connected Thermostat Room/Floor 16 A

WDE011680

WDE011682

The Connected Thermostat Room/Floor 16 A is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water-based heating

Instruction Sheet (PDF)

Device User Guide

Wiser 16 A Relay for Temperature Control

CCTFR6700

Control electrical heaters with On/Off commands (Relay output) or Fil Pilote commands.

Instruction Sheet (PDF)

Device User Guide

Wiser Underfloor Heating Connection Strip

CCTFR6600
CCTFR6610
CCTFR6620

Control thermal actuator valve heads to regulate the flow of hot water in the underfloor pipes.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?