SUG_SV_FI_WH-04

Cybersecurity Principles

These best practices help improve the security of your system by focusing on password management and network configuration.

Password Guidelines

  • Use a combination of uppercase letters, lowercase letters, numbers, and special characters.

  • Ensure passwords are at least 10 characters long.

  • Avoid dictionary words, use a passphrase when possible.

  • Change passwords regularly—at least once a year.

  • Change the default admin password immediately after receiving it or performing a factory reset.

  • Do not reuse passwords across different accounts or systems.

  • Change the default local access password after the first login.

Network Guidelines

  • Connect IoT devices only to your personal home internal network.

  • IoT devices should not be made directly accessible from internet. Ensure that you DO NOT use port forwarding to access an IoT device from the public internet.

  • Place IoT devices on a separate network segment. If your router supports VLANs or other network segmentation, use them.

  • Use the strongest Wi-Fi® encryption available.


Software Guidelines

  • Always use the latest software for all devices in order to get new features, cyber security fixes and improvements.

  • Keep your devices up to date.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?