SUG_SV_FI_WH-04

Automations

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser Home app, you can create automations based on your needs.

Conditions can be:

  • Device status change.

  • Activate away mode.

Times can be:

  • Specific time of a day (e.g. 7:30 each day).

  • Period of time (e.g. from sunrise to sunset).

Actions can be:

  • Change the state of a Device (e.g. open shutter 50%).

  • Send a notification.

  • Activate a Moment.

Limitations:

  • Maximum number of Automations: 10

  • Maximum number of conditions: 10

  • Maximum number of actions: 10

An Automation needs at least one Action and one Condition or specific time of a day.

NOTE: An Automation changes the state of a Device only once, based on the conditions. If you want to reverse the state change, you will have to create another Automation. For example, if you want to switch a lamp based on motion detection, you will have to create an Automation as Presence detected – Light ON and another one No Presence detected – Light OFF.
IMPORTANT: The new action always overrides the current action. Therefore, if a new event is added to the automation or manual operation occurs while a scheduled automation is in progress, the system will stop the ongoing automation. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities.

Automations are created and edited on the Automation screen (A).

You can turn an automation ON or OFF by tapping the slider (B).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?