SUG_SV_FI_WH-04

History

Provides a history of energy sources and energy consumption on an hourly, daily, monthly, and yearly basis, allowing you to track energy usage patterns over time. It also provides a detailed breakdown of energy consumption, enabling you to monitor the usage of individual devices within your system.

  1. On the , tap History to display the Energy sources. This will show you the total energy generated and consumed.

    NOTE: If no energy sources are being tracked, the energy sources data will not be available.

  2. To change the displayed timeframe (hours, days, months, or years), tap (A).

    NOTE: Green bars indicate solar production and gray bars show battery usage.

  3. Tap and select Load consumption to view the energy consumed by individual loads.

  4. Tap (A) again to select a required timeframe.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?