SUG_SV_FI_WH-04

Compatible Wiser Devices for Matter Bridge

Following are the Matter bridge compatible devices:

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Sensors

Wiser Window/Door Sensor

Wiser Water Leakage Sensor

Wiser Motion Sensor

Wiser Temperature/Humidity Sensor

Lights

Wiser Micro Module Light Switch

Connected Relay Switch 10 A

Dimmers

Connected Multiwire Universal Rotary Dimmer LED
Connected Multiwire Universal Push-button Dimmer LED

Wiser Micro Module Dimmer
Wiser Multiwire Micro Module LED Dimmer


Shutters

Wiser Micro Module Shades Control

Connected Blind Control Switch

Appliances

Connected Single Socket Outlet

Connected Wireless Switch 1-gang/2-gang

SmartPlug 16A

Double Socket Outlet 16A

Climate

Wiser Radiator Thermostat

Wiser Room Thermostat

Wiser Underfloor Heating Connection Strip

Wiser 16 A Relay for Temperature Control

Connected Thermostat Room/Floor 16A

Safety

Wiser Smoke Alarm - Battery

Wiser Smoke Alarm 230 V

Energy

PowerTag E

PowerTag C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.