Configuring - flat rate
- After reading the Tariff onboarding information. On the Tariff screen, tap Electricity.NOTE: If you have already configured your tariff settings, follow below menu navigation if you need to modify tariff rate.
On the Home screen, tap . - Tap
(A) and select Flat.
- Tap
(B) to set the contract limit.
IMPORTANT:-
contract limit is already set when pairing the main PowerTag as Grid. Refer to Pairing the main device.
- Select your contract limit (kVA/A/kW) size
from the dropdown menu, then tap
and enter a value using the dial pad as per your country.
TIP: Default value is 20 A with range of 16–63 A.A notification window will be prompted that the Contract Limit is used by Anti-Tripping Management algorithm. If set incorrectly it may not work as expected and could result in the power tripping. Tap Continue, if you like to proceed.
IMPORTANT: Anti-Tripping is applicable only if you have installed Water Heater/EV Socket/Schneider Charge/EVlink Home Smart in your home.For more details, refer to Anti-Tripping (Add Link). - Tap
after setting the contract limit.
-
- Tap
(C) and select a subscription type (D) (refers to recurrent fee).
- Enter a value in the Cost (kr) (E) field and tap Set.
- Tap
(F), enter a flat rate of consumption in the Rate - kr/kWh field and tap Update.
- Tap Save (G).