SUG_SV_FI_WH-04

Updating the firmware

When the hub is connected to the Wiser cloud, it automatically updates the latest firmware. For the first time installation, if you want to check and update the firmware manually, use the app as a professional installer.

To check and update the firmware manually:

  1. Use the Wiser Home App as a professional installer.

  2. Download the latest hub firmware to the app. Refer to Downloading hub firmware into the app.

  3. Follow the steps in chapter Connecting to the Hub's Temporary Wi-Fi® Network .

  4. When asked to connect your hub to your home internet network, tap Skip (A).

  5. You will receive a pop-up notification to confirm your choice. Tap Yes to continue.

  6. Tap Yes, check and update (B) to install the latest firmware.

    NOTE: Tap No, skip if you want to skip the downloading and complete the setup with the current version.
  7. Here are the possible conditions:

    • If the firmware version on your smartphone matches the one on the hub, your setup is complete.

    • If the firmware version on your smartphone doesn't match the one on the hub, the hub will automatically update to the latest firmware version.

      IMPORTANT: The firmware update may take some time. Do not close the Wiser Home App during this process, and ensure that your phone screen remains unlocked. You can set your phone’s Auto‑Lock to Never in the device settings to prevent the screen from locking while the update is in progress.

      If you experience issues with the offline firmware update, refer to the Troubleshooting: Not able to performoffline firmware update.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.