DUG_Radiator Thermostat_WH-06

About the device

The Wiser Radiator Thermostat (hereinafter referred to as Thermostat) uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and switching times are set in the Wiser app.

Personalize your home heating by adding a Thermostat to your Wiser system. These provide effortless control to set different schedules and temperatures in different rooms, and upgrading to room-to-room heating control could save 18% on energy usage. The Thermostat provides individual room control with ultimate comfort, convenience, and practicality.

Features of the Thermostat:

  • Mobile control anytime, anywhere with the Wiser app

  • Works with Amazon Alexa & the Google Assistant

  • Full transparency with Insights and the Heat Report

  • Smart modes for maximum energy efficiency

  • Twist-top boost cap

  • Device user interface lock

Diagram of operating elements

  1. Status LEDs

  2. Radiator Thermostat cap

  3. Ring nut (only used with M30 x 1.5 mm valve adapter)


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?