DUG_IR Controller 1Module-00

About this product

The IR Controller is a control device to automate your home infrared (IR) controlled devices such as televisions, air conditioners, music systems and so on. The device converts mesh network signal to infrared signal.

Key features

  • 360° IR signal coverage.

  • 1 socket for IR extension cables.

  • Supports up to 8 types of IR controlled devices.

Operating elements

  1. Set-up/Reset button

  2. Micro USB port for 5 VDC power supply.

  3. 3.5 mm jack for IR extension cable.

  4. LED indicator.


Suitable install location

IR Convertor can be placed on table or mounted on ceiling to provide desired coverage:

  • Placed on a table provides a surrounding 360° IR signal coverage with a maximum control distance of 8 m.

  • Ceiling mount provides a surrounding 180° IR signal coverage with a maximum control distance of 8 m.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.