DUG_IR Controller 1Module-00

Renaming the device

You can rename the device name using the Wiser app.
To rename the device:
  1. On the Devices page, tap Devices.
  2. Select the IR Controller to change the name.
  3. On the top-right corner of the screen, tap Settings.
    The Hub Settings page appears.
  4. Enter the new name in the Hub Name (A) field.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.