DUG_IR Controller 1Module-00

Removing the device

Using the Wiser app, you can remove an IR controller from the hub's list.
To remove:
  1. On the Devices page, tap Devices.
  2. Tap IR controller.
    The About Hub page appears.
  3. On the top right corner of the screen, tap Settings.
  4. Tap Reset Hub (A).
    A pop-up message appears.
  5. Tap Reset Hub.
    NOTE:
    • When you remove the IR controller, it will delete all connected devices and restore your IR controller to its factory state.

    • By removing the device, you will reset the device. If you still have a problem with the reset, then refer to resetting the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.