DUG_IR Controller 1Module-00

Pairing the device

Connect your mobile device with your home Wi-Fi network and use the Wiser app to access and control it.
To pair the device:
IMPORTANT: Before pairing the device, connect your mobile to the home Wi-Fi network.
  1. Open the Wiser app.
  2. On the Devices page, tap Devices.
  3. Tap + (A) to add a device.
    The Add Device page appears.
  4. The Add Device page includes the following tabs:
    • Preferred (B): This tab allows you to select a device directly from the preferred list.

    • All (C): This tab includes all available devices for you to select from.

    TIP: You can select a device from either tab based on your preference.
    • Select Preferred > SE IR.

    • Select All > Hubs > SE-IR.

  5. Add the following Device Information:
    • Enter Hub Name (D): Add the hub name.

    • Assign Existing Room (E): Select an existing room.

    NOTE: If your room is not in the existing room, create a new one.
    • Add New Room (F): Create a new room.

  6. Tap Next.
  7. Tap Next.
    NOTE:
    • Ensure that your phone is able to discover your preferred Wi-Fi network and SE IR is within 5 meters of your Wi-Fi router.

    • SE IR can connect to a Wi-Fi router with the following specifications:

      • Band: 2.4GHz
        (5GHz is not supported)

      • Security WPA/WPA2
        (WEP is not supported)

  8. Press the reset button 4 times in 10 s using the pin when the LED is solid red.
  9. Tap Next when the red LED indicator blinks rapidly.
    NOTE: To begin scanning for devices, make sure to enable Bluetooth permissions.
  10. Tap MAC ID (G).
    NOTE: If you are unable to find the device, tap Rescan (H).
  11. Tap Select Wi-Fi (I) and choose Wi-Fi network.
  12. Enter the Wi-Fi password in the password field.
    NOTE: After entering the password, the Connect (J) button will be enabled.
  13. Tap Connect (J).
    Now, you can see the newly added hub on the Devices page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.