DUG_IR Controller 1Module-00

Changing the Wi-Fi access point while offline

When you change the SSID or password, the device goes offline. You can connect to a new Wi-Fi network without losing any previous data.
You can change the Wi-Fi network using the Wiser app when the device is offline.
  1. On the Devices page, tap Devices.
  2. Select the IR controller.
  3. On the top right corner of the screen, tap Settings.
  4. Tap Change Access Point.
    Enter Wiser app password pop-up appears.
  5. Enter the Wiser app password.
    The Change Access Point page appears.
  6. Press the reset button 7 times in 10 seconds.
  7. Tap MAC ID.
    NOTE: If you are unable to find the device, tap Rescan.
    It will redirect to the Wi-Fi network which is connected to the mobile.
  8. Enter the new Wi-Fi password in the password field and tap Connect.
    NOTE: The Connect button will be enabled after entering the password.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.