DUG_IR Controller 1Module-00

Using the device

The Control Panel allows you to view device information and control various settings.
On the Devices page, tap Devices and select the device to access the control panel.

The control panel displays the following information:

  • Device information (A)(Name, room, and status)

  • Temperature (B)

  • Brightness (C)

  • Hub information (D) (Type, ID, and firmware version)

  • Hub access point (E)

  • Connected Remotes (F)

  • Settings (G)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.