DUG_IR Controller 1Module-00

Adding IR controlled devices

Add infrared-controlled appliances such as televisions, split system air conditioners, and music systems to an IR Convertor and control them using the Wiser app.

IMPORTANT: If you have a brand-new model of TV, split system air conditioners or HiFi system, the IR code sets may not yet be available in the IR Controller. The code sets in the IR Controller are updated regularly, but there may be times when a new model appliance cannot be used with the device.

NOTE: This task uses the example of adding a television to the IR Controller. The same method can be used to add other infrared-controlled appliances such as split system air conditioners and HiFi systems.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.