DUG_IR Controller 1Module-00

Creating an automation for trigger

Automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automation based on your needs.
  1. On the Actions page, tap Trigger.
  2. Tap + (A) to create an automation.
  3. Tap Add Trigger (B).
    The Select Trigger page appears.
  4. Select a trigger option from the following list on the Select Trigger page:
    • Time (D)

    • Location (E)

    • Device (F)

    • Power (G)

    • Weather (H)

  5. Tap Time (D), select any one of the following options:
    • Any time: Set for any time.

    • At Specific time: Set for a specific time.

    • At in between time: Set for in between time.

    • Perform only once: Set for only once.

    NOTE: Tap the toggle button and then tap Save.
  6. Tap Location (E), select any one of the following options:
    • Arriving location: Select arriving location.

    • Departing location: Select a departing location.

    NOTE: Mobile location should turn on.
  7. Tap Device (F) and select a device from the list.
  8. Tap Power (G) and select an option from the following list:
    • Home EMD

    • Home EMD2

  9. Tap Weather (H) and select an option from the following list:
    • Outside Temperatures

    • Outside Humidity

    • When Sunrises

    • When Sunsets

  10. Tap Add Device (C) and select the device with its respective options from the Devices list (I).
  11. After selecting the device, tap Done (J).
    TIP: Repeat steps 10 and 11 to add more than one device or action.
  12. Enter the Action Name.
  13. Tap Icon and select the icon from the list.
  14. Tap Notification and enable the toggle button for the following options:
    • Show timeline: Displays the total power consumption.

    • Push notifications: Receives the notifications.

  15. Once all the actions are set, tap Save.
    You can see the newly created automation on the Trigger page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.