DUG_IR Controller 1Module-00

Quick (Action)

An action allows you to group multiple actions that are usually done together. Using the Wiser app, you can create actions based on your needs (such as movie night).

To create an action:

  1. On the Actions page, tap Quick.
  2. Tap + to create an action.
    The Add Action page appears.
  3. The Add Action page includes the following options:
    • Add a Sequence (A): Switch on multiple devices in a sequence.

    • Add Quick Action (B): Switch on multiple devices at a time.

  4. Tap Add a Sequence (A) or Add Quick Action (B).
    TIP: Follow the same steps to create an action for both Add a Sequence (A) and Add Quick Action (B).
  5. Tap Add Device (C) and select the device with its respective options from the Devices list (D).
    NOTE: When selecting an IR controlled device, make sure to select the power button to turn it on/off.
  6. After selecting the device, tap Done (E).
    TIP: Repeat steps 5 and 6 to add more than one device.
    NOTE: You can change the waiting time by tapping the time (F) (Only for Add a Sequence).
  7. Enter the Action Name (G).
  8. Tap Icon (H) and select the icon from the list.
  9. Tap Notification (I) and enable the toggle button for the following options and then tap Save (K):
    • Show timeline: Displays the total power consumption.

    • Push notifications: Receives the notifications.

    NOTE: To switch the toggle buttons, make sure to first activate the Notify me toggle button on the settings page.
  10. Once all the actions are set, on the top right-corner of the screen, tap Save (J).
    You can see the newly created action on the Quick page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.