DUG_IR Controller 1Module-00

Technical data

Technical

Adapter input voltage

100-240 V AC

Frequency

50-60 Hz

Adapter output/IR Controller input voltage

5 V DC, 1.5 A

Protocols Supported

Wi-Fi® (2.4 GHz) and IR (Infrared)

Range

Wi-Fi®: up to 30 meters

IR: up to 10 meters (LOS)

Operating Temperature

0° C to 40° C

Dimensions

65 x 65 x 18 mm

65 x 65 x 21 mm (with wall mount bracket)

IR Angle

360 Degrees

Ingress Protection

IP30

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.