DUG_IR Controller 1Module-00

Changing the Wi-Fi access point

You can change the Wi-Fi network using the Wiser app.
  1. On the Devices page, tap Devices.
  2. Select the IR controller.
  3. On the top right corner of the screen, tap Settings.
  4. Tap Change Access Point.
    Enter Wiser app password pop-up appears.
  5. Enter the Wiser app password.
    The Change Access Point page appears.
  6. Select the Wi-Fi network.
    NOTE: If you can’t find your Wi-Fi network, try tapping Refresh (B). If you still cannot find it, you can manually enter the SSID by tapping Enter SSID (A).
  7. Enter the new Wi-Fi password in the password field (C).
    NOTE: The Connect button will be enabled after entering the password.
  8. Tap Connect (D).
    You have successfully connected the new Wi-Fi network.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.