DUG_IR Controller 1Module-00

Using IR remotes

You can add the device using IR Remotes in the Wiser app.
To add the device:
  1. On the Devices page, tap Devices.
  2. Tap +.
  3. Select Devices > IR Remotes > Television
    TIP: You can find all the supported devices as follows:
  4. Select a brand from the list.
    NOTE: Top brands (A) are available on this brand page. Select Search More (B) to find all available brands if you have a different brand.
  5. Tap Power (C) button and then tap Yes (D).
    NOTE:
    • Make sure the hub is near to the television.

    • If the TV does not respond, tap No until the TV responds, and then continue to find other keys accordingly.

  6. Tap the Volume Plus button and then tap Yes.
  7. Tap the Channel Up button and then tap Yes.
    Test Controller pop-up message appears.
  8. Tap Ok (E).
    Now, you can see the remote.
  9. On the top left corner of the screen, tap OK (F) if your device is responding to all buttons on the remote.
    NOTE: If your device is responding to all buttons on the remote, skip step 10.
  10. On the right corner of the screen, tap Not Working (G) if your device is not responding to all buttons on the remote. Select any one of the following option to add:
    • Select model again (H): You can select the model again and try all these steps.

    • Create my Own IR remote (I): You can also create your own remote.

  11. Enter the device name in the name field (J).
  12. Tap Done (K).
    You can see the newly added TV on the Devices page.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.